Haas CNC ControlYears of development have gone into designing the best control hardware and software in the industry. Our new generation machines pack even more innovation into what was already the industry's greatest overall CNC control. To ensure smooth, precise motion control, Haas machine tools use next-generation digital servomotors and high-resolution encoders on all axes. These combine with significant software and motor-control advancements to yield better surface-finish performance than ever before. |
| Haas CNC Control |
Our focus is to provide a robust, dependable control that is seamlessly integrated with the machine. Our closed system is optimized specifically for Haas machines, and does not rely on third-party NC suppliers. When you call Haas, you get a company that takes full responsibility for the entire machine.
The Haas keypad has a full array of keys, including a complete alphanumeric keypad , and all common functions are clearly labeled for operator ease. If you've ever fumbled with hot keys, or had to page through screens looking for a specific function, you will appreciate the simplicity of the Haas control. There are no encrypted codes to memorize.
Common multi-step functions, such as powering-up the machine or setting tool offsets, have been reduced to the push of a single button. Other often-used functions, such as setting work offsets, homing the machine, and selecting the next tool during setup, are also one-button commands.
Most machines use the jog handle only to move the axes around. On Haas machines, the jog handle can also be used in other modes to cursor through the program for faster editing, override spindle speeds and feedrates, or scan through offsets, parameters, etc.
Our full-color, 15" TFT LCD display is designed to work in the machine shop environment. The high-density, high-contrast LCD features a very wide viewing angle, and will not wash out in bright light. The panel is mounted behind anti-glare, tempered glass for protection and easy viewing.
A unique feature of the Haas control is an advanced program editor that allows the operator to edit programs in a dual-window format.
The built-in USB port allows the use of customer-supplied USB flash memory devices or external hard drives.
print
Use the Haas Control Simulator for classroom training and/or on-site control demonstrations. Teach programming and operations using a real, fully upgradable Haas control panel and keypad. Includes simulated dry run graphics, tool length measurement, true DNC and USB convenience. You can also program and download directly from the Control Simulator to Haas machines.
Control Simulator Module Dual Machine
Part: CSMD
Price: $1,695.00