Troubleshooting Guide
Videos
How-To Procedure
Instruction Manual

A Haas Factory Outlet (HFO) can answer your questions, and walk you through your best options.
CONTACT YOUR DISTRIBUTOR >A Haas Factory Outlet (HFO) can answer your questions, and walk you through your best options.
CONTACT YOUR DISTRIBUTOR >A Haas Factory Outlet (HFO) can answer your questions, and walk you through your best options.
CONTACT YOUR DISTRIBUTOR >Set up your Haas mill up to 5 times faster using the Haas Wireless Intuitive Probing System (WIPS). WIPS is a complete probing package that includes the spindle probe, tool setting probe, and optical machine interface, along with powerful software that guides the operator through the job setup process with intuitive, easy-to-use templates.
OVERVIEW
SERVICE DOCUMENTS
VIDEOS
AVAILABLE ON THESE MACHINES
WIPS allows you to quickly and easily define work offset coordinates, set tool length offsets, and perform in-process inspection, for both part inspection and tool breakage detection. WIPS is the single best productivity improvement you can add to your Haas mill.
Troubleshooting Guide
Videos
How-To Procedure
Instruction Manual
Anyone who has run a machine knows how long it takes to set your work offsets. What if you could do it in a fraction of the time? It turns out you can, and it’s easier than you think!
Order the Wireless Intuitive Probing System on any Haas 50-taper VMC, and we’ll include our 50-taper tool load stand for free, allowing you to load heavy and oversized tools quickly, easily, and safely.
The Haas Wireless Intuitive Probing System (WIPS) guides the operator through the job set-up process with easy-to-use templates. The templates help reduce setup time by allowing the operator to multitask while the automatic probing routines are running. WIPS can also ensure that parts and tools are maintained within tolerance throughout the production process, by using the available wear and break-detection routines. WIPS has the ability to define work offset coordinates, set tool length offsets, and perform in-process inspection within the program.
WIPS includes:
Easy-to-use work offset cycles
* Advanced programming methods allow in-process part inspection
Depending on the machine configuration, fixture, or part height, a tool probe riser may be necessary.
Haas provides two options to raise the tool probe from the table to avoid any interference with the workholding or workpiece:
You can order these risers on Parts.HaasCNC.com using part numbers PRB-EC3 or PRB-EC8.
The probes are operated by small programs called probe cycles, which are designed to carry out specific tasks. Each task requires data input, based on the workpiece and the task. Haas Automation provides Visual Programming System (VPS) templates to simplify data entry for calibrating the probe system, setting offsets, and finding the location of rotary tables and tool loaders.
But, the probe system is capable of so much more. With the probe programming manual and a little bit of programming knowledge, you can command the WIPS system to perform these advanced functions:
WARNING - www.P65Warnings.ca.gov
{{=itemTitle}}
Part #: {{=itemSku}}
RETAIL PRICE:
{{ }); }} {{if (itemAllDiscountPrices.length) {}} {{_.forEach(itemAllDiscountPrices, function(dPrice){ }}{{=dPrice.amount}}
WARNING - www.P65Warnings.ca.gov
{{=itemTitle}}
Part #: {{=itemSku}}
{{ } }}RETAIL PRICE:
{{ }); }} {{if (itemAllDiscountPrices.length) {}} {{_.forEach(itemAllDiscountPrices, function(dPrice){ }}{{=dPrice.amount}}
Success! {{=qty}} item(s) added to cart!
Subtotal: {{=sub}}
If you would like more information about how a new Haas machine can bring your products to life, please share your contact information.
All prices and specifications subject to change without notice. Freight, rigging, state & local taxes, vendor installation charges, and dealer installed accessories are not included. Not responsible for misprints or typographical errors. Machines shown with optional equipment. Actual product appearance may differ.
Recently Viewed Items
You Have No Recently Viewed Items Yet
美元价格不包括关税、报关费用、保险费、增值税及运费。
USD prices DO NOT include customs duty, customs fees, insurance, VAT, or freight.
人民币价格包含关税、报关费用、货运保险和增值税, 但不包括运费。
CNY prices include customs duty, customs fees, insurance, and VAT. DOES NOT include freight.
This price includes shipping cost, export and import duties, insurance, and any other expenses incurred during shipping to a location in France agreed with you as a buyer. No other mandatory costs can be added to the delivery of a Haas CNC Product.
KEEP UP WITH THE LATEST HAAS TIPS AND TECHNOLOGY...
HAAS TOOLING ACCEPTS THE FOLLOWING:
This site is protected by reCAPTCHA and the Google Privacy Policy and Terms of Service apply.
2800 Sturgis Rd., Oxnard, CA 93030
Toll Free: (888) 817-4446 / Fax: 805-278-8554